need the following peripherals:SPI,I2C,UART,CAPABILITY TO DRIVE LDC TFT with pixel resolution of 800*480
to load images to the display from the SRAM.
Amal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Amal,
just to clarify, you need more than 2MB of RAM? If so, I'm afraid I don't know of any MCU with that much memory.
You might have to look at some microprocessors that expose the address and data bus to allow scalability with external memory. Possibly something from our Sitara line. http://www.ti.com/processors/sitara-arm/overview.html
I'll move this thread over there.
Thanks,
JD
Hi,
From the processor catalog I can recommend the Sitara AM335x device: www.ti.com/.../overview.html
Hi,
thankyou sir for the suggestion. I have already taken AM3352 series with operating frequency from 300 to 1Ghz.But the problem I am facing now is that the power consumption is too high.
I may have to drop this option only because of this reason.
regards,
Amal
**Attention** This is a public forum