• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » MSP430™ Microcontrollers » MSP430 Ultra-Low Power 16-bit Microcontroller Forum » All Tags » '2553 USB0RXIE UCB0RXIFG
Share
MSP430™ Microcontrollers
  • Forum
  • Announcements
  • E2E Wiki

Browse by Tags

MSP430™ Microcontrollers

Welcome to the MSP430™ Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
'2553 USB0RXIE UCB0RXIFG
  • #include <ti/xdais/ialg.h>
  • '5xx '6xx BSL
  • 'MSP430F1611
  • .bss
  • .h file
  • .hex file
  • .NET
  • .NET MSP-FETU430IF MSP430.dll C#
  • .out
  • .s43 MSP430
  • .text
  • __bis_SR_register(GIE)
  • __enable_interrupt()
  • __even_in_range
  • __MSP430_BASEADDRESS_WDT_A__
  • __segment_begin()
  • __segment_end()
  • __STACK_TOP
  • _bit
  • _c_int00
  • _delay_cycles
  • _system_pre_init( )
  • “Content of Ram”
  • 10bit ADC
  • MSP430
Related Posts
  • Forum Post: '2553 - Programming RX IRQ For USCI_B0 and USART A0 - B0 IRQ Not Set

    johnw johnw
    Hello All, I have programmed a '2553 Value Line part for UART A0 - those IRQ's work fine - but when I set a break point after the following I do not see UCB0RXIE being set - it is still zero: IE2 |= UCA0RXIE + UCB0RXIE + UCB0TXIE; // Enable USCIA0 RX shared interrupt I am using the latest...
    on Apr 25, 2012
  • Forum Post: please clear the errors

    suri naidu suri naidu
    //****************************************************************************** // MSP430G2xx1 Demo - Timer_A, Ultra-Low Pwr UART 9600 Echo, 32kHz ACLK // // Description: Use Timer_A CCR0 hardware output modes and SCCI data latch // to implement UART function @ 9600 baud. Software does not directly...
    on Apr 28, 2012
  • Forum Post: Variable frequency capacitive touch with the MSP430

    Don Bertke Don Bertke
    I noticed that my MSP430 on the Audio/capacitive booster pack came with the inputs all capacitive ready. I noticed that TI is still using the fixed frequency detection algorithm. Is there any chance that they are going to upgrade to the multiple frequency detection capability? I could see a lot of...
    on May 9, 2012
  • Forum Post: i have problem with 16x2 lcd by using msp430g2553,so plz help me or any sample for lcd in "c"

    suri naidu suri naidu
    i have problem with 16x2 lcd by using msp430g2553,so plz help me or any sample for lcd in "c"
    on Jun 14, 2012
  • Forum Post: MSP 430G2553 Sampling in Compare Mode with Timer_A

    Gaurav Kumar1 Gaurav Kumar1
    Hi Friends, I have to sample the input , every 14 microsecond in a 61 micro second slot with the timer input (Project Requirement). I have to do it 8 times to make a byte. More like UART , but I am using it for One Wire Bus communication for my Masters Project. I have written the code as below...
    on Jul 27, 2012
  • Forum Post: Capture MODE Timer_A MSP430G2553

    Gaurav Kumar1 Gaurav Kumar1
    Hi Friends, I have a requirement where I have to capture the falling edge of input signal and when detected ,sample the input the signal exactly at 30 us from the falling edge then again capture the rising edge. If the Rising Edge appears between 480 us from the falling edge , then keep the sampled...
    on Aug 4, 2012
  • Forum Post: How to use properly ADC10 Clock Source Select (ADC10SSELx) from the ADC10 (MSP430G2553)

    Pedro Bacheti Pedro Bacheti
    Hello, I'm using MSP430G2553 to measure the electricity voltage and the electricity current from the supply grid. For I get a good precision I need at least 50 smaples for each cicle (60Hz) in each analog channel (voltage, current). In my following code, I'm using a timer interruption to create...
    on Sep 6, 2012
  • Forum Post: i2c problem

    Sharath Kumar2 Sharath Kumar2
    hi all, i am working on msp430g2553 . can anybody say me the i2c flow of execution when interrupts enabled. I am confused why Tx ISR is required when we are receiving a byte from the master. void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0...
    on Nov 22, 2012
  • Forum Post: MSP430 SPI communication problem with AD7819

    Chu En Ong Chu En Ong
    Hi, Anything wrong with the code below? I can't receive any thing from AD7918 after follow the instruction. The receive enable is set. After I transmit 2 byte to AD7918, it can't enter receive interrupt. Here is my code. #include "msp430x54x.h" unsigned char data[2]= ...
    on Mar 20, 2013
  • Forum Post: MSP430G2553IN20 AND LM35CAZ TEMPERATURE READING PROBLEM

    Debasish Banerjee Debasish Banerjee
    Hello, I am a mere student, and completely new with my new board, I have managed to write the code with assistance from datasheets and google. The code reads the values from INCH_5 and INCH_10 consecutively and sends them via UART so it can be seen via hyperterminal or any of the other serial communication...
    on May 18, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use