I have the following installation:
- Windows Vista, 32-bit
- CCS v4.1.2.000027
- MSP-FET430UIF, hardware="v1.4A", firmware version = v2.01.05.000 (read by Elprotronic's LiteFetPro43 software program)
- Low-level driver: MSP-FET430UIF - VCP (COM8), v6.5.9017.0
- High-level drivers: MSP430.DLL (v2.4.4.0) and HIL.DLL (v1.2.6.0) in c:\Program Files\Texas Instruments\ccsv4\DebugServer\drivers\
The FET tool powers up with an LED sequence of red-red-red-green. I have followed the "Getting Started" section of the CCS User's Guide and created a test project. When ccsv4 attempts to upgrade the firmware of the FET tool it fails at the step of "erasing interrupt vectors..". This error is repeatable on a second Windows PC. I understand that the high-level driver pair is specific to the version of FET tool and the controlling software program, IAR, CCS etc.
Is there a resource/wiki/document that lists the installation requirements by software program (development environment) or can provide some debugging logic for this kind of problem? Thanks.