During product development, we have identified a number of hardware related issues in the use of a Stellaris LM3S1811 MCP including the I2C bus hanging, flash only allowing 100 erase/write cycles, SPI can't be configured to the SPI mode needed by a 25C64 style SPI EEPROM, and a number of other issues that are specified in the datasheet that are noted in the errata (i.e. can't use the internal LDO for the core supply). Do the Tiva TM4C123xxx series MCPs have these issues fixed?