Hello,
I am having had time trying to communicate to my new board with stellaris LM3S5R31 using Ulink2. whenever I try, I get a message that "Erro: Flash Download Failed - Target DLL has bean cancelled". I get this error both through keil ulink2 and TI's ICDI board.However, if i use the LM Flash programmer - Build 1154 , I can program and verify the contents and the MCU works perfectly fine :)
Can anyone suggest me what needs to be done the keil side to get this working. In fact I upgraded to 4.2 and also change the time-out to 500 msec but nothing seems to be working!!
One more thing, I can not communicate even when I select Do not erase and do not program, ie there is nothing to be done, but still get this error when I press the download button!
Any help in this regard to much appreciated.
Thanks in advance
Cross post: http://www.keil.com/forum/19019
Hi Rajan,
Please let me know what revision of LM3S5R31 you are using.
If it is revision C5, refer to the following link for a work around with revision C5
http://e2e.ti.com/support/microcontrollers/stellaris_arm_cortex-m3_microcontroller/f/471/p/109384/386716.aspx#386716
Regards,
Ken
Thanks Ken.
You made my day.
This patch works fine with keil 4.2. Is there a solution for Keil Version: 4.03a? If I try to put this patch onto 4.03a then it hangs up the tool :(
ReagrdsRajan
The patch is only for Keil 4.2.
There is not a solution for Keil 4.03a with revision C5 silicon.