0714.GWY Application Query to TI.pdfWe are using TI Serial to Ethernet code in our product.
Dear All,
We have an application as serial to ethernet at our customer site,
In this application,
SCADA:- Support Serial interface.
Slave Devices: Support Serial Rs-485 Interface.
Serial to Ethernet (Raw)Gateway is used as shown in above application Diagram.
Telnet mode :- Client
Telnet Protocol :- Raw
Please find pdf attachment.
Setting of other product GWY2 but in server mode:-
Problem /Issue:-In this application, if both gateway's are configured IP Mode in DHCP , then both gateway Client and Server IP address may change time to time. In this case, we have to change Remote Telnet port and Server IP address but at client side setting when this case happens
If IP address mode is kept as Static, then above problem won’t come. But customer is not ready to give Static IP for Gateway.
Please suggest me, in DHCP mode, if server IP (& client IP) changes then how it can be made possible that change in IP address in Server should automatically reflect in Client gateway setting ?