ADC with Sequencer Interrupt

Hello,

Im using the stellaris 8962 eval kit . I want to use the adc with the sequencer 3 interrupts with the code as written below 

#include "inc/lm3s8962.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_ints.h"
#include "driverlib/interrupt.h"
#include "driverlib/debug.h"
#include "driverlib/sysctl.h"
#include "driverlib/adc.h"
#include "driverlib/gpio.h"

unsigned long Value = 0;

void ADC3IntHandler(void) //INTERRUPT HANDLER
{
//turn on led
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0x01);
//CLEAR INTERRUPT
ADCIntClear(ADC0_BASE, 3);
//READ DATA
ADCSequenceDataGet(ADC0_BASE, 3, &Value);

}




int main (void)
{

SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_8MHZ);

//GPIO CONFIG
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_0);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0x00);



/////////ADC CONFIGURATION
SysCtlADCSpeedSet(SYSCTL_ADCSPEED_250KSPS);

//Enable clock to the ADC
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);

//DISABLE SEQUENCER
ADCSequenceDisable(ADC0_BASE, 3);

// Configure sample sequence 3: TIMER trigger, priority = 0
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);

//CONFIGURE STEP
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_TS| ADC_CTL_IE | ADC_CTL_END);

//ENABLE INTERRUPTS
ADCIntEnable(ADC0_BASE,3);

//ENABLE THE SEQUENCER
ADCSequenceEnable(ADC0_BASE, 3);

IntMasterEnable();           //Processor Master Interrupt

while(1)
{
ADCProcessorTrigger (ADC0_BASE,3);
}

}//End of Main

,i have modified startup_ccs as the following
extern void ADC3IntHandler(void);
and also changed the name of the interrupt  in the list below as
   ADC3IntHandler,                      // ADC Sequence 3

But the code doesn't work . . .Should i use ADCInt Register function ,if so do give me an example and illustrate how or tell me what steps am i missing 

Regards
Abhay

6 Replies

  • Hello Abhay,

    It looks like you just need to add a IntEnable(INT_ADC0SS3); after your ADCIntEnable() call.

  • Abhay Kothari
    unsigned long Value = 0;

    void ADC3IntHandler(void) //INTERRUPT HANDLER
    {
    //turn on led
    GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_0, 0x01);
    //CLEAR INTERRUPT
    ADCIntClear(ADC0_BASE, 3);
    //READ DATA
    ADCSequenceDataGet(ADC0_BASE, 3, &Value);

    }

    Be careful here, you'll want to take precautions not to let the compiler optimize 'Value'.  Typically that would be declaring any value used between main code and an interrupt as volatile.  In this case you'll get a compiler warning (gcc anyway) because ADCSequenceDataGet(...) is not prototyped as taking a pointer to a volatile unsigned int.  AFAIK, volatile-ness cannot be cast so you cannot get rid of the warning.  Whether or not the compiler would then feel free to optimize 'Value' inside of ADCSequenceDataGet(...), I am not sure, but I would be wary of it.

    You may consider:

    volatile unsigned long Value;

    void ADC3IntHandler(void)

    {

    ADCIntClear(ADC0_BASE, 3);

    unsigned long temp = 0;

    ADCSequenceDataGet(ADC0_BASE, 3, &temp);

    Value = temp;

    }

  • Bit of a pile-up this frequency (post) - do agree with TI Mitch about necessity for ADCIntEnable().

    Beyond that: your code (below) seems not to meet normal/customary Stellaris MCU spec (framed in yellow) for ADC Operation:

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_8MHZ);

    With an 8MHz xtal and PLL bypassed - appears that you are in spec violation.  (never a good idea)

    Note that you seek example & illustrations (for action) - yet provide neither for we attempting to assist!   (True poetic justice - n'est pas?)  

    Your, "Code doesn't work" - doesn't work for we remote diagnosticians either...



     

  • In reply to cb1_mobile:

    Thanks for pointing that out ,but i dont know how to use the PLL,do tell me how to use it . . .when i mean code doesn't work i mean the ADC code 

  • In reply to Abhay Kothari:

    Abhay Kothari
    dont know how to use the PLL

    Almost every example w/in StellarisWare illustrates - also you should focus upon SW-DRL-UG8555 (or newer) which provides just the detail you need.

        ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_25MHZ |
                           SYSCTL_OSC_MAIN);

    Note 2nd pararmeter: SYSCTL_USE_PLL - this enables the PLL.  This function divides the 200MHz PLL by 4 - yielding a 50MHz MCU System Clock.  You require a system clock of 16MHz or greater to comply with TI's ADC spec.

    Final note: "ADC doesn't work" while marginally improving, "doesn't work" - may itself not win many awards for clarity or detail.  Is it off by 2-3 Lsb when converting, occasionally "slip" a conversion, or never converts at all?   (your readers have no clue!)   Can easily list 10 other "doesn't work" - but continue to "argue strongly against" use of such "information-free" phrase.  (quick, uninspired fault descriptions usually will yield poor response...we know that you can do better...)