I have LM4F232H5QD evaluation board.
Whenever i run qs-logger application for collecting Accelerometer data and EK-LM4F232 board is connected to a host PC via
the USB OTG cable then i get exact and fast Accelerometer data from the device.
What i want is to get data from UART0 (PA1 and PA2) using USB TTL.
When i connect EK-LM4F232 board to a host PC via USB-TTL and get data using tera terminal or any other serial terminal,
i get data very slow , like when i shake the board so the changed Accelerometer data comes after 40 second.
Can anyone please tell why this is happening and how can i solve this issue?
Thanks...