• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » Stellaris® ARM® Microcontrollers » Stellaris® ARM® LM3S Microcontrollers Forum » All Tags » S2E
Share
Stellaris® ARM® Microcontrollers
  • Forum

Browse by Tags

Stellaris® ARM® Microcontrollers

Welcome to the Stellaris® ARM® Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
S2E
  • boot_eth
  • bootloader
  • Cortex-M3
  • crossworks
  • Ethernet
  • Finder.exe
  • hub
  • IP address
  • link
  • LM3s6432
  • Luminary
  • MAC Address
  • MAC+PHY
  • MDL-S2E
  • phy
  • RDK-S2E
  • Serial to Ethernet
  • serial2ethernet
  • SPI
  • Stellaris
  • StellarisWare
  • switch
  • TCP/IP
Related Posts
  • Forum Post: Re: Stellaris Serial to Ethernet Questions and Concerns

    Stellaris Paul Stellaris Paul
    If you do not need the line driver connection then you can just use the TX/RX pins and connect them directly to another serial port on another device as long as it does not require rs-232 levels. As far as programming the device, it does come with a flash loader resident on the part but it is a one...
    on May 17, 2010
  • Forum Post: E2S and SPI

    KMJ KMJ
    I would like to know if it's possible to use the Serial-to-Ethernet kit to access a SPI device, in the same way it can provide remote access over ethernet to RS232 devices? I guess using com0com and com2tcp on the PC side, or is something else required? It seem doable, but it had been nice...
    on Jul 1, 2010
  • Forum Post: Some questions about Serial to Ethernet reference design kit

    Wei ennamelocallanguage=维 Wei ennamelocallanguage=维
    Hi,All Some days ago,I got the Serial to Ethernet reference design kit.I have been studying it, and two questions have been bothering me. 1、In the path of "Documentation\Board\S2E_RevC_Board_Package\Layout" of the reference design kit CD, there are some files with a suffix "328"...
    on Aug 10, 2010
  • Forum Post: Re: What's the exact difference between 'pChild' and 'pNext'

    Bill Brown Bill Brown
    Dave, Both recourse 1 and 2 above sound a bit intimidating but I will look into them. Right now I am using the circumflex character as a substitute for the degree symbol. If I could modify that glyph, I'd be in business. But on to simpler things. I have a slider in my interface. Its used...
    on Sep 10, 2010
  • Forum Post: bootloader lost (MDL-S2E)

    leon_DLR leon_DLR
    Hello For assistance with a Stellaris Serial-to-Ethernet Module (MDL-S2E) that worked well but not now. What we did was: We buy only the Stellaris Serial-to-Ethernet Module (MDL-S2E), not the RDK, because the internet shop that sold not told us this need. To make the practices from the PC, we connect...
    on Jul 5, 2010
  • Forum Post: Defining message delimiters on S2E modules

    JethroSmall JethroSmall
    Does anyone have any experience in being able to define message delimiters on the S2E modules? I have a customer who would like to eliminate the overhead of packetizing a single ASCII character for long serial data transmissions. Ideally, he would like to be able to specify the message delimiters (up...
    on Feb 4, 2011
  • Forum Post: Program static IP address of MDL-S2E Client Port

    toby lou toby lou
    Hello- I am using an MDL-S2E module with one serial port configured as a server and the other serial port configured as a client. I would like to be able to programmably (not through the web interface) set a static IP address for the client port. Looking through the documentation and the code,...
    on Feb 24, 2011
  • Forum Post: How to create S2E Extensions

    Patrick Walsh Patrick Walsh
    I would like to create an extension to take serial data and display it in the embedded webpage. Is there a wiki site for the S2E? Has anyone developed similar extensions that I might consider? I've edited the webpages and created an SSI tag in the config.c . Then made a Case for my tag. Then created...
    on Jun 10, 2011
  • Forum Post: makefsfile using -x option

    Patrick Walsh Patrick Walsh
    Can you provide an example of the makefsfile using the -x example? My html editor creates *.bak files that I do not want to include in the file system. I would like to see the full command with the -x as well as the name of the file which holds the list to exclude and contents of that file. ...
    on Jul 14, 2011
  • Forum Post: Re: MDL-S2E board - Ethernet Communication Problem

    Dave Wilson Dave Wilson
    Milap, The default software supplied with MDL-S2E (and RDK-S2E) supports a point-to-point connection between one Ethernet client and one serial device using either the telnet protocol or raw data transfer. The hardware could support multipoint connections but this would require you to rework the software...
    on Nov 28, 2011
  • Forum Post: Re: Rowley CrossWorks Project File for RDK-S2E

    Patrick Langfeld Patrick Langfeld
    Hi Tekkon, I managed to build a project in crossworks for the rdk-s2e! I maintained the same subdirectory structure as used by the other environments (eg keil and ccs). The object and bin files will be placed in an own subfolder named "cw" (for crossworks). I made a "solution"...
    on Jan 19, 2012
  • Forum Post: Cannot know IP address of MDL - S2E device

    akash shekhar akash shekhar
    Hi, We are facing below problem, kindly help us on this issue. We have got MDL-S2E device. It comes with no separate CD or SDK, its just one hardware, no cables, no Ethernet connector board etc. We Assume: -It is ready to use device and we dont need to flash program it anymore as...
    on Jan 23, 2012
  • Forum Post: MDLS2E :cannot send data from telnet terminal to serial terminal

    akash shekhar akash shekhar
    Hi, We are facing below problem, kindly help us on this issue. We are working with MDLS2E device. We executed below steps: -5V Power is applied to device -Connected RX and TX to DB9 male searial cable which is connected to PC. -We connect two hyper terminal one with Serial and another...
    on Feb 13, 2012
  • Forum Post: S2E missing telnet packets

    Matt Fix Matt Fix
    Hi, I'm using the supplied Ti S2E example software w/ the MDL-S2E device. Every once in a while I see a what seems to be a missing telnet message originating on the UART side to be sent out via Ethernet to a PC. Wireshark trace confirms the missed message. Only thing that so far seems to correspond...
    on Feb 29, 2012
  • Forum Post: Re: RDK-S2E module not working via network switch

    Stellaris Miles Stellaris Miles
    When you say "stops working" do you mean that the S2E phy won't link with the switch? Or does it link, but you can't pass traffic? Can you send the model number of the switch you're trying to use? Are you sure your switch is capable of/enabled for negotiating at 10/100? Did...
    on Mar 30, 2012
  • Forum Post: S2E application running on EKS-LM3S8962

    Cristian Marinescu Cristian Marinescu
    I tried to run S2E application, originary from rdk-s2e, on my platform EKS-LM3S8962. Into the source code are some include statements: #include "httpserver_raw/httpd.h" or #include "httpserver_raw/fs.h" #include "httpserver_raw/fsdata.h" and I don't fund them...
    on May 31, 2012
  • Forum Post: S2E problem with servers

    Artur Milota Artur Milota
    Hi! I have a problem with Serial2Ethernet communications with servers. I configure S2E to work in TCP and RAW mode. I have two different servers that my S2E works with. Communication with first server is ok - I get on UART all the data sends back by server (header + body): HTTP/1.1 200 OK Date: Fri...
    on May 27, 2012
  • Forum Post: INT- S2E not establishing connection with Windows 7 PC

    Venkatadri Shantaram84961 Venkatadri Shantaram84961
    Hi I am not able to see S2E connecting to PC through wired network connection. Some time it connects but many times not working. What could be the reason, please sugest. I am following same procedure like in readmefirst. Thanks and Warm Regards Venkat
    on Jul 27, 2012
  • Forum Post: Help For S2E

    Harshal Harshal
    I am supporting to one my customer for S2E, Below are two approaches we are using, a) RS232 signals are given to S2E modules : This approach works well. We are able to change baud rate and able to see data on Ethernet port. The issue is whenever we power off module and again apply the power to...
    on Mar 25, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use