• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Microcontrollers » Stellaris® ARM® Microcontrollers » All Tags » lm3s9b92
Share
Stellaris® ARM® Microcontrollers
  • Forum

Browse by Tags

Stellaris® ARM® Microcontrollers

Welcome to the Stellaris® ARM® Microcontrollers Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
lm3s9b92
  • adc
  • arm
  • boot loader
  • bootloader
  • CCS
  • CCSV4
  • Cortex-M3
  • debug
  • Debugger
  • DK-LM3S9B96
  • EPI
  • Ethernet
  • Flash
  • GPIO
  • I2C
  • IAR
  • interrupt
  • JTAG
  • Keil
  • LM Flash Programmer
  • LM3S3748
  • LM3S6965
  • LM3S6965 Ethernet Evaluation Board
  • lm3s8962
  • LM3S9B90
Related Posts
  • Forum Post: LM3S9B92 flash problem

    Marcel Jost Marcel Jost
    Hi I'm using a LM3S9B92-IQC80-C1 chip on our own hardware. It's running well except the flash control. I cannot erase and write to the flash. Read with the debugger, all flash control register have the value 0x00020000. Is there any known problem with the flash control on this chip...
    on May 25, 2010
  • Forum Post: Re: Monospaced fonts

    Carlo De Bonis Carlo De Bonis
    mdkendall I have used ftrasterize to produce font definition files for several monospaced fonts, including Courier New and Lucidia Console. However, when they are rendered by the graphics library on the display of my RDK-IDM board they are not monospaced (i.e. columns of characters do not line up). Is...
    on May 27, 2010
  • Forum Post: LM3S9B92 Corrupted Bootloader

    Walt White Walt White
    Hello, We can no longer access our IDM-SBC using the ethernet port and LMFlash programmer, and think the bootloader on the board is corrupted. Here is a summary of what happened: We setup a new Stellaris IDM-SBC reference design kit, and ran through several example programs that are included...
    on Jun 8, 2010
  • Forum Post: Re: Re:Serial to Ethernet using LM3S9B92 EVM?

    Frank Field Frank Field
    Bobby, I have just heard from one of my customers with the same challenge. The steps you call out were done however, the port is not complete. It would be nice to have a glimpse of what those minor changes might be? Current symptom is that the web server (for config) stops workng after 10-20 miutes...
    on Jun 17, 2010
  • Forum Post: Problem with hot plugged (VBUS ERROR)

    Andrey Tsybezov52018 Andrey Tsybezov52018
    Hello, Dear Support. I try to develop usb drivers using LM3S9B92 as a USB OTG HOST. I use your example usb_hst_mouse, but I have a problem with hot plugged. Besides, if I connect HID device, which consumption more than 100 mA, arises VBUS ERROR. What to do? Please, help me!!!!!! Sorry for my...
    on Jun 21, 2010
  • Forum Post: Re: Problem with hot plugged (VBUS ERROR)

    Andrey Tsybezov52018 Andrey Tsybezov52018
    Dave, and what about hot plugged? If I connect mouse to host at first time it works normally, but when i disconnect mouse and connect again host does not react! In what a problem?
    on Jun 21, 2010
  • Forum Post: Re: Problem with hot plugged (VBUS ERROR)

    Andrey Tsybezov52018 Andrey Tsybezov52018
    Hi, Dave What about my problem?
    on Jun 26, 2010
  • Forum Post: Ethernet stops working when changing the MAC address on LM3s9b92

    Alea Teeters Alea Teeters
    I am using the LM3s9b92 on a custom board to communicate over ethernet (UDP) to a windows machine running the Hercules utility. I am using LWIP to do this on the chip. The connection has been working well so far, but I've run into a problem when I re-program the MAC address on the LM3s9b92 - the...
    on Jul 27, 2010
  • Forum Post: Error Could not load file 'project.AXF'. Debugger aborted!

    Jean-Baptiste Jean-Baptiste
    Hi, i am in trouble with a LM3S9B92, it was working perfectly well, but after a power off / power on manipulation (brownouts), the MCU did not want to start. now I can load the MCU but i could not start the debugger, and the program does not run. i'm using keil µVision 4 and when i'm...
    on Aug 6, 2010
  • Forum Post: ADC using LM3S9B92

    Dule Sarenac Dule Sarenac
    Dear Sirs, Our company is trying to figure out whether the lm3s9b92 microcontroller would be suitable for our robots. Anyhow, I am running into problems and need help. Currently, I need to set up 2 ADC input channels to monitor the current in our circuit. I need them to monitor whether the current...
    on Aug 9, 2010
  • Forum Post: Re: Re:Linker problem

    darshana garach darshana garach
    Hi, I am having similar errors with linking. I could successfully work with the built-in examples for lm3s9b92 IAR kit, but when I use the FreeRTOS demo, I get the following linker errors: Error[Li005]: no definition for "EthernetIntStatus" [referenced from C:\StellarisWare\boards...
    on Aug 10, 2010
  • Forum Post: How many chip select are there in Lm3s9b92?

    rmznrkn rmznrkn
    I scanned the datasheet, but I confused. I wonder how many external device that I can connect to Lm3s9592 devices by using EPI interface. Could somebody tell me about this thing?
    on Aug 23, 2010
  • Forum Post: Re: LM3S9B92 Flash programming problem

    Stellaris Paul Stellaris Paul
    Unfortunately if you perform an unlock sequence on that device it will erase the patch that is required at the start of flash. This is listed in the errata for the LM3S9B92 Rev C devices( http://focus.ti.com/lit/er/spmz444e/spmz444e.pdf ). In order to resolve your problem, you will need to issue an RMA...
    on Aug 30, 2010
  • Forum Post: LM3S9B92 RTC

    Matthieu Narbonne Matthieu Narbonne
    Hello, I'm looking for get back the date, hour etc from the RTC. How to do it, by software? Thanks Matthieu
    on Sep 1, 2010
  • Forum Post: VDD rise time of LM3S9B92

    BitsMan BitsMan
    First question: In the datasheet of the LM3S9B92, they talk about a VDD rise time (0V-3.3V) of max 10ms under the reset topic. Can somebody explain me what can happen when you not succeed to this requirement, so when the VDD rise time is longer than 10ms? - the internal LDO may not start...
    on Sep 10, 2010
  • Forum Post: LM3S9B92-C3 PHY power down mode

    BitsMan BitsMan
    Dear all, Somebody who knows how to enable the power-down mode of the PHY for the LM3S9B92-C3 devices. For the B1 revision, the " EthernetPHYWrite(ETH_BASE, 0, EthernetPHYRead(ETH_BASE, 0) | 0x0800);" instruction works fine but for the C3 devices this instruction doesn't seems...
    on Sep 10, 2010
  • Forum Post: RDK-IDM-SBC and UART output

    Rajah Rajah
    Hi Guys, I am using an RDK-IDM-SBC kit with an LM3S811 board for debugging. I am using Code Sourcery (arm-none-eabi), eclipse, OpenOCD on ubuntu. Everything works fine, however, I cannot get the UART strings to show on a serial terminal (I use cutecom). When I disconnect the RDK-IDM-SBC board and...
    on Sep 18, 2010
  • Forum Post: Re: hub driver

    Andrey Tsybezov55816 Andrey Tsybezov55816
    Thanks for your help! Now It works! One more question. If to usb hub some devices how to carry out enumeration of devices on ports are connected at once and how to organize work at once all devices via hub? I will be glad to any information)
    on Sep 24, 2010
  • Forum Post: Recovering from CAN Bus Errors

    Allen Moore Allen Moore
    I'm working with a multi-board, CAN-connected system using LM3S9B92, LM3S2B93, and LM3S2793 parts with the Stellaris Peripheral Driver Library. I need to write error-handling code for all the different conditions reported by the CAN Status register (BOFF, EWARN, EPASS, and the LEC codes). However...
    on Oct 7, 2010
  • Forum Post: Re: Random Hard Faults on Wakeup from WFI Instruction (LM3S6918 Running at 50 MHz)

    John Borchard John Borchard
    Thanks for the follow-through, Brian. Do you think this same Sleep problem you documented for the LM3S9B92 would hound the LM3S2793, the target uC I am planning to actually use in my application? jb
    on Oct 8, 2010
  • Forum Post: Programming Issues with Rev C1/C3 of LM3S9B92 & LM3S2B93

    Allen Moore Allen Moore
    We have a four-board (custom) system using LM3S9B92 and LM3S2B93 parts. We started with revision B1 silicon and life was good. No problem programming with Keil's uVision 4.10 (RealView MDK-ARM toolchain 4.12) or with the LM Flash Programmer utility (build 1154). We made a new set of boards to fix...
    on Oct 18, 2010
  • Forum Post: LM3S9B92-IQC80-C3 boot loader not responding to UART0, possible reason?

    Tien-Ren Chen Tien-Ren Chen
    Hello, I'm using a QFP-100 breakout board to evaluate LM3S9B92, I'm trying to use Bus Pirate to talk to the boot loader over UART, but it never respond me with any bytes. The settings I use with Bus Pirate: 115200, 8n1, open-drain output, idle high, pull-up disabled. I tried with the following...
    on Oct 26, 2010
  • Forum Post: Re: Unable to program LM3S9B92

    Nghia Tran Nghia Tran
    I could not find any distributors has LM3SB92 Rev.C3 available. Is there anyway so I can have 5 pieces of LM3S9B92 Rev.C3? Thanks, Nghia
    on Nov 3, 2010
  • Forum Post: How to build the LM3S9B92 eth bootlaoder ?

    gongjian gongjian
    Hi all! I installed the software package of RDK-IDM-SBC-6594 to the directory of C:\StellarisWare.In the directory of boot_loader ,I found there was no project file,so I made a new project and workpalce. I configured the bl_config.h from bl_config.h.tmpl. When building the project, I encountered with...
    on Dec 9, 2010
  • Forum Post: Can anyone please provide support for porting LWIP on ucos ii running on Stellaris LM3s9b92?

    Kiran More1 Kiran More1
    Hi, I am using Stellaris LM3s9B92 uC. My end objective is to have SNMP protocol supported on this uC. On this I am running a ucos ii RTOS. I need LWIP ported on this RTOS as it contains the SNMP support. Kindly help me in this regard. Thx, Kiran.
    on Jun 28, 2012
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use