This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Stellaris Launchpad does not connect to IAR Embedded Workbench 6.4

Hi,

I am trying to run  my code on a Stellaris Launchpad (LX4F120H5QR) using IAR Embedded Workbench. I installed the IAR that came with the package (http://www.ti.com/tool/SW-EK-LM4F120XL).

I opened the workspace C:\StellarisWare\boards\ek-lm4f120xl\ek-lm4f120xl.eww

and tried to download the project blinky.ewp onto the device.

But I get the message: Fatal Error: ***ERROR***Unable to open device 0x00000002 Session aborted!

I have both the USB cables connected to my laptop when I download, and the green power LED is on. In the project settings, the device is chosen as LM4F120H5QR and in the Debugger Setup, the driver is TI Stellaris. 

Any help would be appreciated. Thanks,

Eakta

  • Hi Eakta,

    Have you installed the ICDI drivers? If not, you can find the latest version here: http://www.ti.com/tool/stellaris_icdi_drivers.

    You'll need to download and extract the zip file, then go to the Device Manager and update the drivers for the ICDI devices shown (there should be three in total). Point the driver update dialog to manually search in the folder containing the extracted driver files.

    Regards,

    Sam

  • Surely follow Sam's advice. 

    Beyond that - here are screen caps showing our paid IAR. 

    Note - we have/far prefer JLink probe - likely you direct connect via USB - and perhaps IAR has not caught up yet to new icdi on your board. 

    Compare yours against these - known good...  Note: our MCU differs from yours - general set-up should otherwise be of use...

    Doubt you have JLink - select appropriate for your need.

     

  • In reply to cb1_mobile:

    I have a similar but slightly different and more puzzling problem.

    1. I have an old Stellarise Launchpad (EK-LM4F120XL Kit with LX4F120H5QRFIGA3 chip) and a new Tiva Launchpad (EK-TM4C123GXL Kit with TM4C123GH6PMI chip)

    2. I use IAR Embedded Workbench for ARM, 32K Kickstart Edition 6.60 with standalone permanent license. (Thanks to cb1-mobile's pointer.)

    3. I did install the ICDI drivers (edit).

    4. I cannot use 2.+ 3. to download to neither chips in 1. No error msg is displayed, but Flash contents cannot be changed!

    5. However, I can use 2. to generate a bin file, and use LM Flasher to download that bin file to either chips in 1.

    6. What is more puzzling is, I can now use 2.+3. to debug. This include setting breakpoints, single stepping, etc.

    I can live with this situation. Actually, I kind of like it. But still, it is very puzzling.

  • In reply to Sam Friedman:

    Thank you Sam. That was the key.

  • Guru 47910 points

    In reply to old_cow_yellow:

    @OCY:

    old_cow_yellow
    No error msg is displayed, but Flash contents cannot be changed!

    That's disturbing.  Is any form of message flashed/displayed - as this download fails?   And - if you review my screen cap (above) - might the IDE have ticked "suppress download?"  While you, "like the extra LM Flasher step" - does it not delay - and force extra (non-seamless) effort? 

    My sense is that your download should succeed w/your LX4F120 MCU - provided you've followed (above) screen caps - AND have selected (or have) the correct download file.

  • In reply to old_cow_yellow:

    old_cow_yellow

    5. However, I can use 2. to generate a bin file, and use LM Flasher to download that bin file to either chips in 1.

    6. What is more puzzling is, I can now use 2.+3. to debug. This include setting breakpoints, single stepping, etc.

     Hi OCW, I fear this is inappropriate for you, I got caught a couple of time:

    debugger set to hardware or simulator? IAR default to simulator.

     Regards

     Roberto


     Please login & click    Verify Answer    if this post answered your question.

  • In reply to cb1:

    @OCY:

    Unclear if you have & use JLink or route USB cable directly from PC to target board.  Earlier caps - intended for op - covered JLink usage.

    Sure that you know - but (just in case) and to benefit others who may employ IAR w/out JLink - here my best guess of key: Project > Options - settings.

    Note: Below cap shows my switch away from (earlier) JLink to TI Stellaris.  (have not tried - this is my best sense...)  Note the .ddf file - mated to your MCU.  I do not operate the IDE w/that overide default box ticked - did so here to reveal that particular file...

    And following cap reveals that while our MCUs differ - same flashloader file is used.  Again - override default ticked so that filename reveals...

    Somewhere we have that LX4F120 board - although the crippled nature of that MCU discouraged our use.  If these caps don't fix your issue - kindly advise & I'll search/find and perform live test/verify...

  • In reply to cb1_mobile:

    cb1,

    Thanks. Indeed, I did not set up IAR correctly. I thought that not checking "Supress download" means allow download and "Use flash loader's" means I need something else. I was wrong. This works:

    -- OCY

  • In reply to old_cow_yellow:

    @OCY,

    Good for you!   Sometimes too many options/choices confound.

    The acuteness of your, "issue description" led to this quick solution.

    I'd tick, "Verify Download" (just in case).  Note that you can, "Debug with and without Download." (adjacent,  top right icons)

    The many features of IAR really "bubble up" via a 2nd monitor - if mountain passes allow - that may blip your radar...

  • In reply to cb1_mobile:

    cb1,

    Yes. I did try "Verify Download" before I checked "Use Flash loader(s)". IAR did not send error or warning even though the Flash was clearly not programmed.

    I also tried "Verify Download" when I checked "Use Flash loader(s)".  IAR did not send error or warning either. In this case the Flash was programmed correctly. (Hence this does not proof that they did verify it!)

    -- OCY

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.