The latest version of Tivaware has a pin_map.h file that appears to be missing the USB0 DP and DM pin definitions for the TM4C123GH6PZ part. When using the Pinmux application, it generates the following as part of the pin initialization:
//
// Enable port PJ0 for USB0 USB0DM
//
MAP_GPIOPinConfigure(GPIO_PJ0_USB0DM);
MAP_GPIOPinTypeUSBAnalog(GPIO_PORTJ_BASE, GPIO_PIN_0);
//
// Enable port PJ1 for USB0 USB0DP
//
MAP_GPIOPinConfigure(GPIO_PJ1_USB0DP);
MAP_GPIOPinTypeUSBAnalog(GPIO_PORTJ_BASE, GPIO_PIN_1);
However, there is no definition for GPIO_PJ0_USB0DM or GPIO_PJ1_USB0DP in pin_map.h or anywhere else I can find.
Is this an oversight? What should the value in pin_map.h be?