Hello!
I'm working with the EK-TM4C1294XL Launchpad and trying to figure out how to use the hardware PWM module.
Ideally I'd like to find a way to use it in energia, but my guess is that energia doesn't support chip specific features like that, sadly. So any help getting it set up in CCS 6 would be fantastic.
So far I've made a new project and tried to compile the tivaware pwm example "dead_band.c" with an added #define PART_TM4C1294NCPD
Code I've tried is copied here:
//***************************************************************************** // // dead_band.c - Example demonstrating the dead-band generator. // // Copyright (c) 2010-2014 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // // This is part of revision 2.1.0.12573 of the Tiva Firmware Development Package. // //***************************************************************************** #define PART_TM4C1294NCPD #include <stdbool.h> #include <stdint.h> #include "inc/hw_memmap.h" #include "driverlib/gpio.h" #include "driverlib/pin_map.h" #include "driverlib/pwm.h" #include "driverlib/sysctl.h" #include "driverlib/uart.h" #include "utils/uartstdio.h" //***************************************************************************** // //! \addtogroup pwm_examples_list //! <h1>PWM dead-band (dead_band)</h1> //! //! This example shows how to setup the PWM0 block with a dead-band generation. //! //! This example uses the following peripherals and I/O signals. You must //! review these and change as needed for your own board: //! - GPIO Port B peripheral (for PWM pins) //! - M0PWM0 - PB6 //! - M0PWM1 - PB7 //! //! The following UART signals are configured only for displaying console //! messages for this example. These are not required for operation of the //! PWM. //! - UART0 peripheral //! - GPIO Port A peripheral (for UART0 pins) //! - UART0RX - PA0 //! - UART0TX - PA1 //! //! This example uses the following interrupt handlers. To use this example //! in your own application you must add these interrupt handlers to your //! vector table. //! - None. // //***************************************************************************** //***************************************************************************** // // This function sets up UART0 to be used for a console to display information // as the example is running. // //***************************************************************************** void InitConsole(void) { // // Enable GPIO port A which is used for UART0 pins. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Configure the pin muxing for UART0 functions on port A0 and A1. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX); // // Enable UART0 so that we can configure the clock. // SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // // Select the alternate (UART) function for these pins. // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // Prints out 5x "." with a second delay after each print. This function will // then backspace, clearing the previously printed dots, and then backspace // again so you can continuously printout on the same line. The purpose of // this function is to indicate to the user that the program is running. // //***************************************************************************** void PrintRunningDots(void) { UARTprintf(". "); SysCtlDelay(SysCtlClockGet() / 3); UARTprintf(". "); SysCtlDelay(SysCtlClockGet() / 3); UARTprintf(". "); SysCtlDelay(SysCtlClockGet() / 3); UARTprintf(". "); SysCtlDelay(SysCtlClockGet() / 3); UARTprintf(". "); SysCtlDelay(SysCtlClockGet() / 3); UARTprintf("\b\b\b\b\b\b\b\b\b\b"); UARTprintf(" "); UARTprintf("\b\b\b\b\b\b\b\b\b\b"); SysCtlDelay(SysCtlClockGet() / 3); } //***************************************************************************** // // Configure the PWM0 block with dead-band generation. The example configures // the PWM0 block to generate a 25% duty cycle signal on PD0 with dead-band // generation. This will produce a complement of PD0 on PD1 (75% duty cycle). // The dead-band generator is set to have a 10us or 160 cycle delay // (160cycles / 16Mhz = 10us) on the rising and falling edges of the PD0 PWM // signal. // //***************************************************************************** int main(void) { // // Set the clocking to run directly from the external crystal/oscillator. // TODO: The SYSCTL_XTAL_ value must be changed to match the value of the // crystal on your board. // SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ); // // Set the PWM clock to the system clock. // SysCtlPWMClockSet(SYSCTL_PWMDIV_1); // // Set up the serial console to use for displaying messages. This is just // for this example program and is not needed for PWM operation. // InitConsole(); // // Display the setup on the console. // UARTprintf("PWM ->\n"); UARTprintf(" Module: PWM0\n"); UARTprintf(" Pin(s): PD0 and PD1\n"); UARTprintf(" Features: Dead-band Generation\n"); UARTprintf(" Duty Cycle: 25%% on PD0 and 75%% on PD1\n"); UARTprintf(" Dead-band Length: 160 cycles on rising and falling edges\n\n"); UARTprintf("Generating PWM on PWM0 (PD0) -> "); // // The PWM peripheral must be enabled for use. // SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0); // // For this example PWM0 is used with PortB Pins 6 and 7. The actual port // and pins used may be different on your part, consult the data sheet for // more information. GPIO port B needs to be enabled so these pins can be // used. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // // Configure the GPIO pin muxing to select PWM functions for these pins. // This step selects which alternate function is available for these pins. // This is necessary if your part supports GPIO pin function muxing. // Consult the data sheet to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PB6_M0PWM0); GPIOPinConfigure(GPIO_PB7_M0PWM1); // // Configure the GPIO pad for PWM function on pins PB6 and PB7. Consult // the data sheet to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using. // GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_6); GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_7); // // Configure the PWM0 to count up/down without synchronization. // Note: Enabling the dead-band generator automatically couples the 2 // outputs from the PWM block so we don't use the PWM synchronization. // PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC); // // Set the PWM period to 250Hz. To calculate the appropriate parameter // use the following equation: N = (1 / f) * SysClk. Where N is the // function parameter, f is the desired frequency, and SysClk is the // system clock frequency. // In this case you get: (1 / 250Hz) * 16MHz = 64000 cycles. Note that // the maximum period you can set is 2^16 - 1. // TODO: modify this calculation to use the clock frequency that you are // using. // PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, 64000); // // Set PWM0 PD0 to a duty cycle of 25%. You set the duty cycle as a // function of the period. Since the period was set above, you can use the // PWMGenPeriodGet() function. For this example the PWM will be high for // 25% of the time or 16000 clock cycles (64000 / 4). // PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, PWMGenPeriodGet(PWM0_BASE, PWM_OUT_0) / 4); // // Enable the dead-band generation on the PWM0 output signal. PWM bit 0 // (PD0), will have a duty cycle of 25% (set above) and PWM bit 1 will have // a duty cycle of 75%. These signals will have a 10us gap between the // rising and falling edges. This means that before PWM bit 1 goes high, // PWM bit 0 has been low for at LEAST 160 cycles (or 10us) and the same // before PWM bit 0 goes high. The dead-band generator lets you specify // the width of the "dead-band" delay, in PWM clock cycles, before the PWM // signal goes high and after the PWM signal falls. For this example we // will use 160 cycles (or 10us) on both the rising and falling edges of // PD0. Reference the datasheet for more information on dead-band // generation. // PWMDeadBandEnable(PWM0_BASE, PWM_GEN_0, 160, 160); // // Enable the PWM0 Bit 0 (PD0) and Bit 1 (PD1) output signals. // PWMOutputState(PWM0_BASE, PWM_OUT_1_BIT | PWM_OUT_0_BIT, true); // // Enables the counter for a PWM generator block. // PWMGenEnable(PWM0_BASE, PWM_GEN_0); // // Loop forever while the PWM signals are generated. // while(1) { // // Print out indication on the console that the program is running. // PrintRunningDots(); } }
But that generates the error:
"../main.c", line 98: error #20: identifier "GPIO_PA0_U0RX" is undefined "../main.c", line 99: error #20: identifier "GPIO_PA1_U0TX" is undefined "../main.c", line 214: error #20: identifier "GPIO_PB6_M0PWM0" is undefined "../main.c", line 215: error #20: identifier "GPIO_PB7_M0PWM1" is undefined
I am betting I have the define incorrect or something, since I assume the example is meant to be easy to use, but I'm stuck and would really appreciate some help here.
Thank you!
Garrett