I am using a 3.2in LCD display that has a ssd1289 controller. It is interfaced to my mcu via a 8-to-16 bit adapter to save a few GPIO pins. I was wondering if there was a way to set up the TM4C123 DMA controller to continuously write data to the LCD. My problem is that the ssd1289 requires control signals before receiving each pixel data therefore requiring the use of the CPU to drive the signals. So would this be possible or am I overreaching with the hardware i have?