I'm using a TM4C129x chip. I have external flash on the SSI bus running in legacy mode. The flash will output its busy status on its SO line (MCU's SI) when CE (chip enable) is pulled low. (I'm manually running the CE line in code) Is it possible to read the SSInRX pin state via the gpio data register when the pin is configured for SSI operation?
Thanks,
Mike