hi, here is a screen shot:
doesn't driverlib.lib have the files to take care of this error? Any help would be great. Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi, here is a screen shot:
doesn't driverlib.lib have the files to take care of this error? Any help would be great. Thanks
The function that is undefined/unresolved is SystemInit. This is not a driverlib function It is coming from startup_tm4c123.s this file is usually the interrupt table and other init stuff from the compiler.
This looks like an issue on the Keil side not the DriverLib side.
thanks for the help so far. Anyone know where I find step be step instructions? I know the problem is in the finer details of starting a new project and in the options. Is tivaWare 2.1 compatible with Keil 4.73? I copied most of the settings from a working example. The only setting I couldn't just type was in the options...Linker tab...Scatter File. So, I made a new file...name it TryAgain.sct...copied the code from a working example. Then I compiled I got a different error:
Build target 'Target 1'
assembling TryAgain.sct...
TryAgain.sct(25): error: A1355U: A Label was found which was in no AREA
".\TryAgain.axf" - 1 Error(s), 0 Warning(s).
Target not created
I used Keil in a edx microcontroller course and liked it more than ccs. I'm having this problem because we never went over starting a new project from scratch.