Hi all,
According to Zhaohong's reply to my previous question, "After a power-on-reset, CPU starts exection from ROM. If it sees that the flash iserased (the content at flash address 0x4 is 0xffffffff), CPU will enter the ROM bootloader. It will wait for the activities from one of the following ports: EMAC, I2C, SSI, UART, and USB to start bootloading"
I erased 1294 launchpad via CCS->Tools->On Chip Flash->EraseFlash then ran LM Flash program, but neither the ethernet nor serial nor USB could find the 1293 launchpad.
Could anyone be so kind to give me a pointer?
Thanks!