Hello ,
I am developing a product using TIVA TM4C129ENCPDT,
I want to communicate two devices each having a TM4c129ENCPDT controller on them using ethernet.
One device will act as master and request data from the other device which will act as slave.
Which example code i need to follow.?
I got the enet_lwip , enet_io , enet_uip code with dk-tm4c129x board but they all work as server .
Also my knowledge on interfacing ethernet with microcontroller is very less.
So which will be best way to proceed? Are there any other sample code to which i can refer.
Also i want to implement encryption for the data being transferred in future.
Any help will be very useful.
Thanks
Any help will be very useful