Hi
I am trying to generate a pwm signal of 25khz period. and 0 to 100% duty cycle variation. But i do not see 0-100% variation in pwm duty cycle. the duty cycle and pulse width count relation is 0% - 170 , 66% - for 400 and above.
Below is the code. I have used the code from the example.. I change the pulse width count manually for now.
void main(void)