Hai
currently i am working on TM4C123GH6PM micro controller,and here i have interfaced my micro controller to the GSM modem.And when i transmitting the command AT from my controller then it has to generate an interrupt in that interrupt handler i want to store only the "RESPONSE" of interrupt handler,but here i got the problem is the same data is also stored in side the buffer in the interrupt handler i.e what i send(same AT).......please help me about this issue.....thank u
here just i modified uart echo example....
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/uart.h"
unsigned char ok[]="OK\r\n";
unsigned char m[20];
int count=0;
int count1=0;
unsigned int i,j;
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
// The UART interrupt handler.
/************************************************************/
void
UART1IntHandler(void)
{
uint32_t ui32Status;
++count1;
//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART1_BASE, true);
//
// Clear the asserted interrupts.
ROM_UARTIntClear(UART1_BASE, ui32Status);
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART1_BASE))
{
m[count]=ROM_UARTCharGetNonBlocking(UART1_BASE);
count++;
if(count==20);
count=0;
}
ROM_IntDisable(INT_UART1);
}
/********************************************************/
int
main(void)
{
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// //instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPUEnable();
ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Enable processor interrupts.
//
ROM_IntMasterEnable();
//
// Set GPIO B0 and B1 as UART pins.
//
GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);
ROM_GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART1_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
//
// Enable the UART interrupt.
ROM_UARTIntEnable(UART1_BASE, UART_INT_RX | UART_INT_RT);
ROM_UARTFIFOEnable(UART1_BASE);
UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX1_8, UART_FIFO_RX1_8);
UARTEnable (UART1_BASE);
while(1)
{
do
{
tx("AT\r\n");
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
}while((strcmp(ok,m))!=0);
do
{
tx("AT+CREG=1\r\n");
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
}while((strcmp(ok,m))!=0);
do
{
tx("AT+CREG=?\r\n");
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
SysCtlDelay(SysCtlClockGet());
}while((strcmp(ok,m))!=0);
}
}
void tx(unsigned char *p)
{
while(*p!='\0')
{
ROM_UARTCharPutNonBlocking(UART1_BASE, *p);
p++;
}
ROM_IntEnable(INT_UART1);
}