I am new to embedded programming and this forum, as far as posting is concerned but have used it a lot to debug my code and get used to the tiva environment. I thank everyone who have contributed.
I have a question now, was not able to find a solution so thought of posting it here.
Initially i can burn a code onto the board, but after that when i send a command to update, to the board.
It must be able to receive the compiled code via uart1 or spi1, or for the sake of simplicity let us assume that a compiled code is available on the SD card that is plugged in.
Now it must update the code so that it can, from now on run the new compiled code.
Is it possible ? If yes how ?
And also after updating it must start running the new code. How is that to be done ?
Should it be reset oris there any other way ?
As i said, i am new to embedded programming, so a simple explanation accompanying a complicated explanation (if any) would greatly help.
Thanks in advance..