I am using the TM4C123G as a bulk device with DFU options. This uses the Composite Device - as shown in the examples - as a wrapper or container of sorts for the Bulk Device and DFU Device.
The standard DFU driver under the provided windows_drivers folder worked for this setup, but I had to adjust the bulk device driver INF file in order to get Windows to recognize it as the driver for this device. This causes an "unsigned driver" error that is rather painful to ignore in Windows 8 and 10. Is there a signed driver example of the USB Bulk Device as device 0 in a composite device setup? Or is this something that must be customized and signed on our end?
Thank you in advance,
John