Dear Sir,
I want to make the Frequency Generator with High Accuracy in range between 0.0005 Hz to 20 Hz with the accuracy of microHz ie. 1.00001
I have tried with the 32bit concatenate Timer bit I put the Counts as per frequency with the formuale of ((ui32SysClock / (frequency_Hz)) / 2); where frequency_Hz is the Frequecny which we want to give as output now It will do that accordingly but it doesnt give me proper accuracy of micro Hz and it flucatues the Output freq.
Can you please suggest me how to got such accuracy with now fluctations.