I tried to implement a TFTP protocol in the EK-TM4C1294NCPDT board, using the files tftp.c and tftp.h contained in the utils folder on TivaWare 2.1.3.156. I want to read the value of specific memory position in the flash via TFTP.
As there are not examples of this protocol for my board, I use the enet_io example and I modifying for add a TFTP protocol implementation. I initialize the TFTP using TFTPInit function, as it is in the code below:
int main(void) { uint32_t ui32User0, ui32User1; uint8_t pui8MACArray[8]; // // Make sure the main oscillator is enabled because this is required by // the PHY. The system must have a 25MHz crystal attached to the OSC // pins. The SYSCTL_MOSC_HIGHFREQ parameter is used when the crystal // frequency is 10MHz or higher. // SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ); // // Run from the PLL at 120 MHz. // g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000); // // Configure the device pins. // PinoutSet(true, false); // // Configure debug port for internal use. // UARTStdioConfig(0, 115200, g_ui32SysClock); // // Clear the terminal and print a banner. // UARTprintf("\033[2J\033[H"); UARTprintf("Ethernet IO Example\n\n"); // // Configure SysTick for a periodic interrupt. // MAP_SysTickPeriodSet(g_ui32SysClock / SYSTICKHZ); MAP_SysTickEnable(); MAP_SysTickIntEnable(); // // Configure the hardware MAC address for Ethernet Controller filtering of // incoming packets. The MAC address will be stored in the non-volatile // USER0 and USER1 registers. // MAP_FlashUserGet(&ui32User0, &ui32User1); if((ui32User0 == 0xffffffff) || (ui32User1 == 0xffffffff)) { // // Let the user know there is no MAC address // UARTprintf("No MAC programmed!\n"); while(1) { } } // // Tell the user what we are doing just now. // UARTprintf("Waiting for IP.\n"); // // Convert the 24/24 split MAC address from NV ram into a 32/16 split // MAC address needed to program the hardware registers, then program // the MAC address into the Ethernet Controller registers. // pui8MACArray[0] = ((ui32User0 >> 0) & 0xff); pui8MACArray[1] = ((ui32User0 >> 8) & 0xff); pui8MACArray[2] = ((ui32User0 >> 16) & 0xff); pui8MACArray[3] = ((ui32User1 >> 0) & 0xff); pui8MACArray[4] = ((ui32User1 >> 8) & 0xff); pui8MACArray[5] = ((ui32User1 >> 16) & 0xff); // // Initialze the lwIP library, using DHCP. // lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP); // lwIPInit(g_ui32SysClock, pui8MACArray, 2887557220, 4294934528, 2887526654, IPADDR_USE_STATIC); // // Setup the device locator service. // LocatorInit(); LocatorMACAddrSet(pui8MACArray); LocatorAppTitleSet("EK-TM4C1294XL enet_io"); uint32_t i; for(i = 0; i < 99; i++) { buffer[i] = 'a'; } buffer[99] = '\0'; // // Initialize a sample httpd server. // httpd_init(); TFTPInit(okToContinue); // // Set the interrupt priorities. We set the SysTick interrupt to a higher // priority than the Ethernet interrupt to ensure that the file system // tick is processed if SysTick occurs while the Ethernet handler is being // processed. This is very likely since all the TCP/IP and HTTP work is // done in the context of the Ethernet interrupt. // MAP_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY); MAP_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY); // // Pass our tag information to the HTTP server. // http_set_ssi_handler((tSSIHandler)SSIHandler, g_pcConfigSSITags, NUM_CONFIG_SSI_TAGS); // // Pass our CGI handlers to the HTTP server. // http_set_cgi_handlers(g_psConfigCGIURIs, NUM_CONFIG_CGI_URIS); // // Initialize IO controls // io_init(); // // Loop forever, processing the on-screen animation. All other work is // done in the interrupt handlers. // while(1) { // // Wait for a new tick to occur. // while(!g_ulFlags) { // // Do nothing. // } // // Clear the flag now that we have seen it. // HWREGBITW(&g_ulFlags, FLAG_TICK) = 0; // // Toggle the GPIO // MAP_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, (MAP_GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1) ^ GPIO_PIN_1)); } }
I created the callback functions, but now I implemented only the TFTPInit and pfnGetData Callback.
tTFTPError getDataFromTFTP(struct _tTFTPConnection *psTFTP){ unsigned long ulOffset; UARTprintf("Get block %d, %d\n", psTFTP->ui32BlockNum, psTFTP->ui32DataLength); // // Where does this block of data get read from? This is calculated from // the requested TFTP block number. // ulOffset = ((psTFTP->ui32BlockNum - 1) * TFTP_BLOCK_SIZE); // // Copy the data into the supplied buffer. // memcpy(psTFTP->pui8Data, (unsigned char *)(buffer + ulOffset), psTFTP->ui32DataLength); // // Tell the caller everything went fine. // return(TFTP_OK); } tTFTPError putDataFromTFTP(struct _tTFTPConnection *psTFTP){ return TFTP_OK; } void closeTFTP(struct _tTFTPConnection *psTFTP){ } tTFTPError okToContinue(struct _tTFTPConnection *psTFTP, bool bGet, int8_t *pui8FileName, tTFTPMode eMode){ psTFTP->pfnClose = closeTFTP; // // Is this a GET or PUT request? // if(bGet) { // // GET request - fill in the image size and the data transfer // function pointer. // psTFTP->pfnGetData = getDataFromTFTP; psTFTP->ui32DataRemaining = 100; } else { // // PUT request - fill in the data transfer function pointer. // psTFTP->pfnPutData = putDataFromTFTP; } return TFTP_OK; }
The board got the IP adress and the http server worked perfectly. But when I use a native TFTP client in the windows, the TFTPRecv function and the pfnGetData callback function is called. But the TFTPRecv function is called , when the TFTPDataRecv function should be called, and occurs the Fault_ISR when udp_recv in the line 618 is called again.
Why the function TFTPDataRecv is never called?