Other Parts Discussed in Thread: ADC161S626EVM, , TM4C1294NCPDT
Tool/software: Code Composer Studio
I'm trying to use the booster pack from TI the ADC161S626EVM with the LaunchPad through the SSI on the BoosterPack 1 Pins, but in the pin_map.h, doesn't have the proper configuration pin for CS, which would be the SSI2FSS on pin PE4. Instead, the library has the SSI2FSS on pin PD2 (#define GPIO_PD3_SSI2CLK 0x00030C0F) which is located in the BoosterPack 2 pins. How will I be able to connect/configure the CS pin in the board?