Hi,
the TM4C1294NCPDT has 256 kB of SRAM which one would expect in an address region of 0x4.0000 bytes. This is also the case in the .gel file available in CCS where the SRAM region is declared as below to start at 0x2000.0000 and be of 256 kB in size:
GEL_MapAddStr(0x20000000, 0, 0x00040000, "R|W", 0); /* SRAM */
However, the respective manual shows a different, larger non-power-of-2 range in two places: "0x2000.0000 0x2006.FFFF Bit-banded on-chip SRAM" in Table 2-4. Memory Map and Table 2-5. Memory Access Behavior.
More or less the same was also mentioned here already.
Is this just an error in the documentation or what's else at these addresses? May I kindly request some changes to the documentation in this regard? Thanks.