Tool/software: TI-RTOS
Hello,
I'm using
- CCS Version: 6.1.0.00104,
- TIRTOS: tirtos_tivac_2_16_01_14,
- xdctools_3_32_01_22_core
and i want to change the link status/activity LED from (PF4 <==> LED1 & PK4 <==> LED0) to my external port using my CPLD which is connected to Port P to extend the I/O of the micro-controller. currently with PF4/PK4 i'm using MAP_GPIOPinConfigure/GPIOPinTypeEthernetLED but how can i configure driver to use my external port on the CPLD for the two LEDs?
Thanks,
Mohammed Fawzy