I need to use IntEnable(INT_TIMER6A); inside a generic library which should work for either TM4C123 or 129.
Well, INT_TIMER6A expands to INT_CONCAT(INT_TIMER6A_, INT_DEVICE_CLASS) and, if there is no p/n defined in the library (as is the case), further goes to:
#define INT_DEVICE_CLASS "UNKNOWN"
Causing the error
function INT_RESOLVE declared implicitly
Is there a (simple) solution for that?
For further reference, this thread asked something on the same theme, but there is just a generic explanation there, yet not the solution.
Regards
Bruno