Hello Community
I started a simple blink project and it is working nicely.
I made some code myself as I am trying out the architecture and did not edit or added anything about clock frequency. I was expecting to have the default frequency of 16Mhz as stated in the documentation and some videos from TI.
In ATMEL (ATMEGA) the F_CPU if not set will automatically run the MC at 8MHZ, which is the default internal oscillator. So I was expected that here we have something similar.
Yet my board runs at 1,6MHz. any suggestions? Is it a default 1,6Mhz when nothing is set up? Is there no way avoiding setting up the SysTime?
I am using a very simple delay loop.
Yes I know I should not do it, I should set up a timer and use the SysTime or interrupts. Yes I know I should use the API and not play with registers myself.
Thank you for your answer.