Other Parts Discussed in Thread: UNIFLASH
Hi,
I have a problem with custom board, using a TM4C1294NCPDT.
Here is the error message :
CORTEX_M4_0: GEL Output:
Memory Map Initialization Complete
CORTEX_M4_0: Error connecting to the target: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
Tried on 3 different boards, all have the same message.
But, 2 years ago using the same setup, one of the same boards worked perfectly.
Anything that I need to check ?