Other Parts Discussed in Thread: EK-TM4C1294XL, TM4C1294NCPDT,
Hi,
I have programmed a serial to Ethernet converter and have tested it successfully on EK-TM4C1294XL Launchpad. Now I have shifted to a custom board designed fir this facility. When I run the code, Ethernet is detected on my PC and the LED on custom board also glows. I am also able to acquire the static IP for the board, But I am not able to open the configuration webpage from the acquired IP. Also I am not able to get any ping of PC with the device.(I checked using MS-DOS). I visualised the data using wireshark utility.
Also here I am able to detect Ethernet on my laptop . I am sending the ICMP packet from my laptop's ip: 192.168.1.130 to the static IP assigned to the custom made board: 192.168.1.5. For the board, the subnet mask is 255.255.255.0 and the default gateway is 192.168.1.1.
For my laptop, the subnet mask is 255.255.255.0 and the default gateway is 192.168.1.1.
But, when I connect it to the Launchpad, everything works fine with the same code. I am also getting response ICMP packet from the board to the laptop's ip.
What can be the error? IS there some error in configuration or the hardware?
Regards,
Apoorv