The HIB module for all purposes is seemingly disabled by conditions in both pin handling columns (acceptable / preferred) of table 26-7.
Yet does the acceptable practice for unused HIB module pins (table 26-7) allow the HIB module to assert Tivaware peripheral sleep commands and put peripherals to sleep when commanded to do so?
Or does the HIB module not have explicit control of the peripheral sleep function as logical deduction would have us think it should?
Seemingly line powered peripheral sleep modes are not being disclosed in the datasheet HIB module section 7 or in the architectural overview section 1.