Tool/software: Code Composer Studio
Am trying to get a Windows 10 CCS v7 environment fully up and running. For the moment, trying to build some examples for the EK-TM4C129EXL...
Having tested with a few sample apps - which all build successfully - I consistently get a 'total freezeup' of CCS at the point it should be uploading the firmware. CCS becomes unresponsive.
Do not see the debugger break at main loop, as would be standard ( right? )
CORTEX_M4_0: GEL Output: Memory Map Initialization Complete CORTEX_M4_0: Error connecting to the target: Unable to communicate with the device. Please check your connection.
Unplugging the EK-TM4C board then releases CCS, but reports error in communication with board.
I do have drivers installed; Device Manager reports:
Stellaris Virtual Serial Port (COM6) -- and
Stellaris ICDI DFU Device
Stellaris ICDI JTAG/SWD Interface
Please note that the same board is programmable - and debug-able - from OSX.
Hmmm.... What am I missing?