Other Parts Discussed in Thread: TM4C129ENCPDT
Tool/software: TI-RTOS
Hi,
we have custom design board. In our project we are saving data to EEPROM on power Fail Detection. by using capacitors we are able to generate 400 ms time after power fail detect. we are able to store data to EEPROM most often But still sometimes we are not able to write data to EEPROM during that interval. for a note our custom board have GSM Modem interfacing using UART.
My question is
1. How much Time EEPROM write will take to write 100 Bytes data on fixed location?
2. In TM4C129ENCPDT controller data sheet it is mentioned "Program time for 32 bits of data with memory space available is Normally 110 us and Max 600 us" in that "space available" word used what it means? should we have to erase data before writing?
3. Another line is "Program time for 32 bits of data in which a copy to the copy buffer is required, the copy buffer has space and less than 10% of EEPROM endurance used" in this "copy to copy buffer" means? Is it copying data from one EEPROM location to another?
4. i am using "if(sys_state.eeprom_error = (char)EEPROMInit())" for validate EEPROM writing but it will give success always. any solution?
Thanks.