Other Parts Discussed in Thread: UNIFLASH
Our EVB used 2 TM4C129XNCZAD and when our test the power on/on in the -40 degC the one of TM4C129XNCZAD can't boot up successfully.
We tried to reflow this TM4C129XNCZAD and remount it (remount TM4C129XNCZAD BGA balls) back to the PCB, the all test results are cold boot fail.
We have checked the TM4C129XNCZAD power up/down sequence (power, clock, reset) are meeting to the spec.
In -40 degC chamber we used JTAG to download or verify image by UniFlash that all work normally, but when we used Tiva to run the part of main code it shows failure information as below:
『CORTEX_M4_0: Can't Run Target CPU: (Error -1268 @ 0x1090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0).』
Until we replaced the new one TM4C129XNCZAD and re-test in the -40 degC chamber, the new one TM4C129XNCZAD works and can be booted up normally, therefore we think it means this one TM4C129XNCZAD maybe had been damage.
We need to know what happen in this one and what kind of reason can cause it cold boot fail under the spec.?