Tool/software: TI C/C++ Compiler
Hi all:
I had issue about RTC follow is my test
platform : EK-TM4C123GXL
RTOS:TI RTOS Tivac 2 16 00 08
IDE:
Code Composer Studio 7.3.0
XDCtools 3.32.0.06_core3
Compiler TI v16.9.4.LTS
void InitHibernation(void) { SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE); // // Wait for the Hibernate module to be ready. // while(!SysCtlPeripheralReady(SYSCTL_PERIPH_HIBERNATE)) { } // // Determine if the Hibernation module is active. // HibernateEnableExpClk(SysCtlClockGet()); // Configure the clock source for Hibernation module and enable the // RTC feature. // HibernateClockConfig(HIBERNATE_OSC_HIGHDRIVE); HibernateRTCEnable(); }
and i print the HibernateRTCGet() value to console. Follow is my log.
2018/5/23 17:22:30 [RX] - RTC:172 <CR><LF>
2018/5/24 09:20:25 [RX] - RTC:58329 <CR><LF>
58329 - 172 = 58157 = 16 h 09 m 17 s
2018/5/23 17:22:30 + 16 h 09 m 17 s
= 2018/5/24 09:31:47
over the actual time 11 m 22 s
Is any RTC register setting wrong? or need to be set?
Thank you.