This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8850: Vpropi resistor to gnd

Prodigy 310 points

Replies: 1

Views: 260

Part Number: DRV8850

Hi,

we are using the DRV8850 to drive a linear motor. When designing the PCB, the following question arose:

The chip has this VPROPI pin that is connected via 1k to GND in our application according to TI proposals. As we don’t need to read the H-bridge current and that particular resistor is currently an issue at the PCB, we would like to know if it is safe to omit it and leave this pin just unconnected.

Thank you for your support.

Best Regards

Kevin den Toom

  • Kevin,

    According to current setting equation R(VPROPI)=2000 x VCC 1 V / IOUT. If R(VPROPI) is open, the IOUT would be zero.
    So, please add that resistor.

    Best Regards,

    Wang Li

    Motor Drive Solutions

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.