This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

no part number

Intellectual 360 points

Replies: 5

Views: 173

Hi,


Would you please guide me where i can find an 'example with document' about
"Sensor less indirect field oriented control (IFOC) for 3-Phase Induction Motors (ACIM) with IQ-Math C2000”?
(In Application Report, SPRABP9–October 2013, only the direct (rotor) flux oriented control System with flux and open-loop speed estimators is described.)


Best wishes,
Jean

  • Ali, I am not familiar with in-direct FOC, i have forwarded it to motor control team for additional comments.
  • In reply to Manish Bhardwaj:

    For 3-phase ACIM control, the TI reference design used indirect rotor flux oriented control scheme for sensored-FOC, and direct rotor flux oriented control for sensorless-FOC. So there is no such "Sensorless indirect field oriented control (IFOC) for 3-Phase Induction Motors (ACIM) with IQ-Math C2000” reference design now.

    You might download controlSUITE and find the related document and reference code in below folders if you install it by default.
    Indirect scheme Sensored-FOC: C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVACI_Sensored
    Direct scheme Sensorless-FOC: C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVACI_Sensorless
  • In reply to Yanming Luo:

    Hi Luo,

    Thank you for your answer. i have searched in ControlSUITE before and i couldn't find anything about the subject too. But these two links are so useful.

    Anyway i want to use "Sensorless IFOC" because i have read in papers that it has better performance in cases such as: Lower drift and lower temperature effects and better response in low speed. Is it true?

    I need an algorithm with lowest torque ripple and best response in very low speed for 5 to 7 KW ACIM.

    Which algorithm do you suggest if i design my own estimator (e.g. kalman)?
    What is the limitation and problem of sensorless IFOC that TI does not use yet?

    Thank you
  • In reply to Manish Bhardwaj:

    Thank you so much Manish.
    it is my pleasure to hear your suggestions and advises either for the rest of discussion . because it is related to DFOC too.
    Thank you
  • In reply to Yanming Luo:

    Anyway i want to use "Sensorless IFOC" because i have read in papers that it has better performance in cases such as: Lower drift and lower temperature effects and better response in low speed. Is it true?

    I need an algorithm with lowest torque ripple and best response in very low speed for 5 to 7 KW ACIM.

    Which algorithm do you suggest if i design my own estimator (e.g. kalman)?
    What is the limitation and problem of sensorless IFOC that TI does not use yet?

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.