This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8881: Toff Period

Prodigy 90 points

Replies: 1

Views: 72

Part Number: DRV8881

Customer question:

"The DRV8881 describes a Toff time. From the datasheet it seems like Toff only comes into affect once the current threshold is hit. Does the Toff period also occur any time the PWM cycle goes low?

For example blue is the PWM signal with a 1us period. When it goes low, does Toff apply for 10, 20, or 30us until the output is driven high again with the next positive PWM pulse?"

  • Hi Sagar,

    You are correct. Once the current threshold is reached, the device switches to off time. The off time can be slow decay, mixed decay, or fast decay.

    Please note the output PWM frequency is determined by many factors, such as VM, VREF, sense resistor, and motor parameters. The frequency may change at each step in the indexer table.

    Have you considered using the DRV8886AT instead? If it meets your voltage and current requirements, the device is easier to use and requires fewer external components?

    Rick Duncan
    Motor Applications Team

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.