This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Linux/DRV2605: How to control an ERM using the Linux input subsystem

Prodigy 50 points

Replies: 11

Views: 493

Part Number: DRV2605

Tool/software: Linux

I am trying to test the DRV2605 using an ERM with the Linux driver (github.com/.../drv260x.c) installed. On startup the motor works during calibration, however I am unable to get it to work by writing to the device file as described in www.kernel.org/.../ff.html. Test code below

#include <stdio.h>
#include <fcntl.h>
#include <string.h>
#include <errno.h>
#include <unistd.h>

#include <linux/input.h>
#include <sys/ioctl.h>

#define BITS_TO_LONGS(x) \
        (((x) + 8 * sizeof (unsigned long) - 1) / (8 * sizeof (unsigned long)))
unsigned long features[BITS_TO_LONGS(FF_CNT)];

int main(const int argc, const char **argv)
{
    int fd;

    if (argc != 2) {
        printf("usage: %s <device-file>\n", argv[0]);
        return 1;
    }

    fd = open(argv[1], O_RDWR);
    if (fd < 0) {
        printf("Error opening file '%s': %s\n", argv[1], strerror(errno));
        return 1;
    }

    int num_effects;
    if (ioctl(fd, EVIOCGEFFECTS, &num_effects) < 0) {
        printf("Error getting number of effects playable at the same time: %s\n", strerror(errno));
        return 1;
    }
    printf("%d effects playable at the same time\n", num_effects);

    struct ff_effect effect = {
        .type = FF_RUMBLE,
        .id = -1,
        .direction = 0,
        .trigger = {0, 0},
        .replay = {
            .length = 1000,
            .delay = 0
        }
    };
    effect.u.rumble.strong_magnitude = 0x7F;

    if (ioctl(fd, EVIOCSFF, &effect) < 0) {
        printf("Error creating new effect: %s\n", strerror(errno));
        return 1;
    }
    printf("New effect ID: %d\n", effect.id);

    struct input_event play = {
        .type = EV_FF,
        .code = effect.id,
        .value = 3
    };

    if (write(fd, (const void*) &play, sizeof(play)) < 0) {
        printf("Error writing effect to file: %s\n", strerror(errno));
        return 1;
    }
    printf("Wrote effect\n");

    return 0;
}

 The program runs fine with no errors but nothing happens to the ERM. 

  • Hi,

    Welcome to E2E and thank you for your interest in our products!

    Have you verified if the device files are created according to the 5.2 section? It seems that the utility fftest is also required to test the driver:

    Best regards,
    Luis Fernando Rodríguez S.

  • In reply to Luis Fernando Rodriguez S.:

    Hi Luis, thanks for your reply. The input device is loaded - the relevant segment from /proc/bus/input/devices is pasted below

    I: Bus=0000 Vendor=0000 Product=0000 Version=0000
    N: Name="drv260x:haptics"
    P: Phys=
    S: Sysfs=/devices/soc0/soc/30800000.aips-bus/30a30000.i2c/i2c-1/1-005a/input/input1
    U: Uniq=
    H: Handlers=event1 evbug 
    B: PROP=0
    B: EV=200001
    B: FF=1 7030000 0 0

    Unfortunately I don't have fftest on my device although I will look into it

  • In reply to h:

    I managed to get fftest on the device and ran it:

    Force feedback test program.
    HOLD FIRMLY YOUR WHEEL OR JOYSTICK TO PREVENT DAMAGES
    
    Device /dev/input/event1 opened
    Features:
      * Absolute axes: 
        [00 00 00 00 00 00 00 00 ]
      * Relative axes: 
        [00 00 ]
      * Force feedback effects types: Periodic, Rumble, Gain, 
        Force feedback periodic effects: Square, Triangle, Sine, 
        [00 00 00 00 00 00 00 00 00 00 03 07 01 00 00 00 ]
      * Number of simultaneous effects: 16
    
    Setting master gain to 75% ... OK
    Uploading effect #0 (Periodic sinusoidal) ... OK (id 0)
    Uploading effect #1 (Constant) ... Error: Invalid argument
    Uploading effect #2 (Spring) ... Error: Invalid argument
    Uploading effect #3 (Damper) ... Error: Invalid argument
    Uploading effect #4 (Strong rumble, with heavy motor) ... OK (id 1)
    Uploading effect #5 (Weak rumble, with light motor) ... OK (id 2)
    Enter effect number, -1 to exit
    0
    Now Playing: Sine vibration
    Enter effect number, -1 to exit
    4
    Now Playing: Strong Rumble
    Enter effect number, -1 to exit
    5
    Now Playing: Weak Rumble
    Enter effect number, -1 to exit
    -1
    Stopping effects

    I tried playing the effects that were uploaded OK and still no luck

  • In reply to h:

    Hi,

    Sorry for late response. I'm following up on this thread.
    Are you still facing difficulties to test our device? What is the current status?
    Have you tried something else additional to the information provided above?

    Thanks and Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • In reply to Ivan Salazar:

    I have managed to make some progress. On debugging the driver I found the work queue wasn't running the queued function that was supposed to play the driver. I have rewrote much of the driver to configure it as a simple character device instead of an input device so I can write waveform sequences to it. This was a functionality missing from the supplied driver and I couldn't find an obvious way to use the input subsystem to play any specific waveform number so if you know any way to do this that would be preferred to my customised driver solution. Unfortunately I made quite a number of different changes to the driver so couldn't say exactly what caused it to work (I am relatively new to Linux kernel development).

  • In reply to h:

    I am sorry to hear you're having trouble using our device driver. We fully support the Hardware solution although the driver is not being actively supported.
    Please let us know if you have additional questions.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • In reply to h:

    HI,

    May I know how you found fftest.

    If possible, can you please share the binary.

    My platform is ARM based linux. 

    Regards,

    Vijay

  • In reply to Vijay Kumar76561:

    I got the source from here: https://github.com/flosse/linuxconsole/tree/master/utils. You only need fftest.c and bitmaskros.h to compile. I cannot share the binary sorry but it was easy enough to cross compile (using a custom Yocto SDK) since you only need those two files.

  • In reply to h:

    Thanks for sharing the information.

    The device on which this needs to be integrated is an android based device.
  • In reply to Vijay Kumar76561:

    Hi,

    Thanks for sharing this information with the community.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.