• TI Thinks Resolved

CCS/BOOSTXL-DRV8301: Updating variables with values from GUI

Prodigy 240 points

Replies: 3

Views: 75

Part Number: BOOSTXL-DRV8301

Tool/software: Code Composer Studio

Which line of the code that update the values of global variables such as, 'gMotorVars.Flag_enableSys', '  gMotorVars.PosStepInt_MRev', '  gMotorVars.PosStepFrac_MRev' etc. with the values given from the GUI? . [I'm dealing with InstaSPIN Motion 'Lab 13e'.].

  • Hi Abdul,

    Can you please confirm the software your are using? Are you using motorware 18? We do not support GUI anymore with the motorware 18. Do you mean CCS debug window? Thanks.

    Han

  • In reply to Han Zhang6:

    Hi Han Zhang,

     Yes I mean the CCS debug window. I'm using "motorware_1_01_00_18".

    Thank you.

  • In reply to Abdul Rasheed28:

    Hi Abdul,

    Regarding the CCS debug window, it does not require any code to change the data of variables in watch window. It is through JTAG and directly change the value in memory.

    If you have a specific function that you are trying to implement, please specify. Thanks.

    Han