This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Can the DRV8662 be used to drive a piezo buzzer as an alarm?

Prodigy 130 points

Replies: 1

Views: 1839

Can the DRV8662 be used to drive a piezo buzzer as an alarm?

The traditional alarm circuit uses an inductor or auto transformer in parallel with the piezo buzzer to resonate and generate a high voltage.

Is the DRV8662 a suitable alternative?

See the schematic at the top of page 6 for the existing approach to driving the piezo buzzer:

http://www.diodes.com/datasheets/ZSD100.pdf

See also the schematic:

http://www.quasarelectronics.co.uk/kit-files/electronic-kit/3015.pdf

The question is whether the TI IC can replace the T1 autotransformer which is a physically large part?

 

  • Hi, LL:

    from software perspective, you may need some PWM or DAC output to feed the DRV8662.

    please check the below diagrams.

     

    Thanks

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.