This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8308 EVM - Detailed Specs for TelcoMotion DT4260-24-055-04H-TI motor

Prodigy 175 points

Replies: 2

Views: 2938

The DRV8308 EVM has an included TI custom motor from Telcomotion that is designated as: TelcoMotion DT4260-24-055-04H-TI. 

I have been unable to locate any detailed specs on the motor from the TI website nor Telcomotion's web site for this motor.

What I am looking for is the following kind of information

    - Number of pole pairs

   - Min/Max/Nominal voltages

   - No load speed

   - No Load current 

   - Stall current

   - Stall torque

  - Signal Pinout diagram 

Could you either post those here to the forum, or point me to a PDF that has those specs.

Thanks

    Wayne

  • Hi Wayne,

    The file is located in the Hardware: DRV8308EVM zip file. This can be found in the DRV8308EVM folder.

    Rick Duncan
    Motor Applications Team

  • In reply to Rick Duncan:

    Rick:
    Got it.
    Thank you for such a quick response.
    Much appreciated !
    Wayne

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.