This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV10987: DRV10987 shows no output

Prodigy 680 points

Replies: 5

Views: 326

Part Number: DRV10987

From e2echina:

Motor does not spin. DRV10987 seems no output.

Schematics as attached.

Here is the read/write soft code (e2 read/write correct):

DRV10987_Write_Byte(0x60 , 0x8000); // motor stop

DRV10987_Write_Byte(0x31 , 0x0000); // write 0x31 to 0x0000  

DRV10987_Write_Byte(0x31 , 0xC0DE); // write 0xC0DE to 0x31

Delay_10ms();
Delay_10ms();
Delay_10ms();

Receive_Sum_Value = DRV10987_Read_Byte(0x32); // 

if (Receive_Sum_Value==0x01)
{

DRV10987_Write_Byte(0x90 , 0xC001); // 
DRV10987_Write_Byte(0x91 , 0x0049); // 
DRV10987_Write_Byte(0x92 , 0x00C1); // 
DRV10987_Write_Byte(0x93 , 0x37B8); // 
DRV10987_Write_Byte(0x94 , 0x3BAF); // 
DRV10987_Write_Byte(0x95 , 0x7840); // 
DRV10987_Write_Byte(0x96 , 0x007A); // write shadow register

DRV10987_Write_Byte(0x35 , 0x0006); // sync shadow register to EEPROM 


Delay_1s();

Receive_Sum_Value = DRV10987_Read_Byte(0x32); // wait for EEPROM write ends 

if (Receive_Sum_Value==0x01)
{

DRV10987_Write_Byte(0x35 , 0x0002); // sync EEPROM to shadow register 

Delay_10ms();
Delay_10ms();
Delay_10ms();

Receive_Sum_Value = DRV10987_Read_Byte(0x32); // wait for sync ends 

if (Receive_Sum_Value==0x01)
{

Receive_Sum_Value = DRV10987_Read_Byte(0x90); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x91); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x92); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x93); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x94); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x95); // read byte
Receive_Sum_Value = DRV10987_Read_Byte(0x96); // read byte

Delay_10ms();
Delay_10ms();
Delay_10ms();


DRV10987_Write_Byte(0x60 , 0x0000); // motor spin 
}

}

}

   

  • There could be a variety of issues so let's narrow it down:

    1) Check the board is functioning properly in stand-by mode by doing the following:

    -See if Vcc pin on board =24V. Vreg = 5V, V3P3 = 3.3V, check what Icc is, speed spin = 1.6V. Let me know the values.

    -If the part is a sleep mode device, then the voltage on speed pin voltage needs to be greater than 2.2V. Right now its 1.6V, so needs to be higher.

    2) Check if its a device eeprom  setting issue

    -Check if your device is hitting any locks. Disable the sleep/standby mode as well.

    Let me know first if those things help fix your issue.

  • In reply to Sanmesh Udhayakumar:

    Hey Alvin,

    Were you able to explore the issue further or go through my debugging steps?

    Sincerely,
    Sanmesh U.
  • In reply to Sanmesh Udhayakumar:

    It's Nation Day golden week here now. I didn't get any feedback. Hopefully we can hear from customer next week.

    Thank you.

  • In reply to Alvin Zheng:

    Hey Alvin,

    Let me know if you were you able to explore the issue further or go through my debugging steps.

    Sincerely,
    sanmesh U.
  • In reply to Sanmesh Udhayakumar:

    Did not get any update yet. Close for now. Thank you.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.