Other Parts Discussed in Thread: MSP430G2553, ,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you very much for the reply Wang Li, I had seen this already but my query is more related to where can I get the ref. design of the whole system. I understand that ref. design of most of the blocks is available by clicking on them but many of them don’t show the used MCU and even if the MCU is used in the ref. design it varies from say LED driver ref. design to CAN ref. design so can you please point me to a single ref. design that has a single MCU as shown in the block diagram interfacing all the different parts like LIN CAN , POWER supply, MUX etc…??
Thanks for the reply, the MCU is highlighted in the second option under the drop down which is base BCM with the gate way , but clicking on the same gives the same reference design as for the gateway
I was thinking DRV for the FET driver portion
Siddharth,
Our reference designs typically are for subsystems in the applications. In general, we do not develop full system reference designs. Further, if a reference design is targeted for automotive applications, we will automotive-qualified ICs in the design.
Can you please let me know in which reference design you are seeing DRV8307?
With regard to processors, TI has processors for BCMs which have gateway function integrated in them or for standalone gateways. These applications require much higher computational power and so TI's Jacinto processors are a good fit for these applications.
Arun
Siddharth,
With reference designs, in some cases TI is showing solutions for analog portions of the PCB and in others digital portions. If the goal of the design is to show analog solutions, the reference designs may use processors if needed and the processor itself is not the focus of the design. If is up to the customer to take relevant portions of TI Designs including suitable processor and build the full system.
Arun
Thanks in that case can you please suggest a suitable ref. design around Jacinto ?