described as the tittle
the DRV8704 chip's V5 pin is shorted with GND and the chip is heating
the design is: STM32 chip generate pwm ,control the sleep pin-reset pin-CS pin at 3.3V level ,iso7241 is used to translate the 3.3v-level into 5V-level ,3.3v and 5v is isolated by iso7241.
the VM of DRV8704 is 24V.
when i measure the V5 pin ,it drop down to 0v from 5v. cut off power, i found that the V5 pin is short with GND.
i check the circuit and PCB design, no errors found.
so i confused.
if the V5 short with GND ,there maybe shorting pin.i do not find it.the status regsister set is default.
so, i want to ask ,in which case the V5 short with GND?