This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC Motor drive IC recommended

Other Parts Discussed in Thread: DRV8873, DRV8871, DRV8870, DRV8872

hi, Drive a brushed-dc motor 24V 1A, the power supply is 24V, realize a positive turn and a reverse turn, the main circuit protection circuit, overcurrent, overload, motor drive and MCU isolation or protection, so the circuit is not easy to burn IC, so I want to know about the manufacturers of some solutions and Suggestions, thank you!

      PS:ET-SGM37D-24120  Motor parameters are as follows

     Best Regards

    mydy

  • Shu,

    First let us check what does the brushed DC motor selection tool give us?

    1. change the Vs max voltage to >28V. It gives us 33 parts

    2. I would think an integrated FET solution is good for 1A application. So, I set the FET Rds-on to 400mohm. And then, we have 10 parts.

    Open the selection result, I would pick DRV8873_Q1 because of more integrations; new release and auto-qualification. I would think all motor drive parts have several protection methods to meet customer requirements. So, you can pick other parts according to your system requirement.

  • Shu,

    Rick pointed out if we relaxed the Rds-on to 600mohm, we can find the most simple and low cost part DRV8870; DRV8871 and DRV8872 can meet your requirement.
    DRV8870 uses external power current sense resistor to sense the winding current.
    DRV8871 has internal current sense resistor.
    DRV8872 has fault pin to report fault condition.
    All those three parts can support 24V 1A application.