Dear Support-Team,
We are using three DRV8833 motor drivers to drive an inductive load. To protect the load, we make use of the DRV8833 current chopper at 100mA (maximum rating for load). From the datasheet:
When an H-bridge is enabled, current rises through the winding at a rate dependent on the DC voltage and
inductance of the winding. If the current reaches the current chopping threshold, the bridge disables the current
until the beginning of the next PWM cycle. Immediately after the current is enabled, the voltage on the xISEN pin
is ignored for a fixed period of time before enabling the current sense circuitry. This blanking time is fixed at 3.75
μs. This blanking time also sets the minimum on time of the PWM when operating in current chopping mode.
So, immediately after the current is enabled (meaning high level on the xIN pin?), the current on the xISEN pin is ignored for 3.75us. Does the bridge still conduct during that time? We need to drive the load at 3.9kHz with a minimum on-time of 1us.
Kind regards.