This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353RS-EVM: VGS_Status 2: SA_OC: Indicates overcurrent on phase A sense amplifier (DRV8353xS)

Part Number: DRV8353RS-EVM

Hi,

I'm trying to test the Evaluation Board DRV8353RS-EVM. From Start everything was Ok until i connected the BLDC-Motor to the board.

The gate driver tried to identify the Motor parameters, but after about 30 seconds it didn't work anymore.

Then n-fault-LED lights up and the fault is Indicates overcurrent on phase A sense amplifier (DRV8353xS).


Did anyone see have the fault ?  is it still posible to resolve this problem?

Thanks for your help!

Best regard,

Hoang