Other Parts Discussed in Thread: DRV10983
Hi,
I am trying to setup the DRV10983-Q1 to input current of 1.5A and Input voltage ranging from 6.2V to 25V.
So far when I program the chip to closed loop the input current being received from the power supply is a maximum of 0.12A at an input voltage of 12V.
Thanks
Mohammad